Welcome to Würth UK For trade customers only

Rust remover

View our wide range of brochures here!

FIGHT RUST WITH PROFESSIONAL PENETRATING OILS

Würth is recognized for the quality of its penetrating and rust removers for professionals intended for multiple uses:

PENETRANTS FOR MULTIPLE FIELDS OF APPLICATIONS

The ""Multi"" penetrating oil is a penetrating oil which can be applied to many areas of application. It is able to dissolve rust on nuts, screws, bolts, locks and other assemblies. In addition, it lubricates locks, hinges, chains, etc. It cleans and maintains plastic and metal parts. It prevents corrosion of metal parts and repels moisture in electrical blocks, relays, sockets, cable connections, etc.

HIGH POWER PENETRATING ORGANO-MOLYBDENUM DEGREASER (ROST OFF PLUS)

Rost off Plus is a top-of-the-range penetrating oil intended for light vehicles, heavy goods vehicles, two-wheelers, agricultural machinery, public works machinery, garden machinery, industry, merchant marine and pleasure craft, etc. It is particularly ideal for overtightened, rusted or seized assemblies such as bolts, axles, studs, sleeves, etc.

COLD DEGREASER WITH IMMEDIATE EFFECT (ROST OFF ICE)

Rost Off Ice goes even further than Rost off Plus. This cold penetrating oil is specially designed for very heavily rusted or seized assemblies. It is suitable for all sectors of activity such as heavy or light vehicles, agricultural and public works machinery, industrial maintenance, merchant or pleasure marine where the parts are often very strongly oxidized because in contact with salt water.

PENETRANTING OILS FOR INJECTORS

Würth injector penetrating oil makes it easier to remove injectors seized with soot and carbon, turbos and all engine parts that are carbonated.

HOW DOES RUST OCCUR? HOW DOES A RUST REMOVER COMBAT THIS?

Rust is a constant problem in the workshop and in material handling machines. It is the corrosive damage that occurs when iron and steel react with water and oxygen. In this case, the material cracks, becomes damaged and must be completely replaced. Rust should therefore always be avoided by preventive measures and careful maintenance of all iron and steel parts. However, it is not always possible to avoid it. Once rust sets in, it can become a real problem. But fortunately, there are Würth products for this.

Rust can occur in many places. If the rust attack is evident, repair and maintenance measures should be taken. Sometimes, however, rust is not noticed until it is already too late. It is particularly inconvenient with screws and fasteners. Nuts are particularly susceptible to rust. Rust attack is usually not detected and can spread. But if the rust has progressed too far, the fastening element cannot be loosened. It therefore wastes time on a daily basis.

It is precisely for these cases that the penetrating agent is suitable. It manages to eradicate rust after application. This way rusted screws can be unscrewed again.

Würth offers various penetrating agents for this purpose. These include penetrating agents that work with OMC2 additive technology.

Other anti-rust penetrating agents cool the material and cause cracks in the rust. There are also penetrating agents specially adapted and approved for use in food-related fields. The intended use should be the deciding factor in choosing the appropriate penetrating agent.

Discover our other related product ranges: Rust converter, Anti-rust for vehicle, Cutting and drilling oil...