Welcome to Würth UK Solo para profesionales

Blind rivets

View our wide range of brochures here!

Clasificación

Productos populares
Productos más populares en la categoría Blind rivets

THE BLIND RIVET, A FIXING ELEMENT WHICH MAKES THE ASSEMBLIES NON-REMOVABLE
 

A blind rivet is a fastener used to assemble materials permanently. At Würth, we have designed a wide range of blind rivets for professionals: exploded, fluted, petal, structure ... This article will tell you a little more about their characteristics.


 
HOW DOES A BLIND RIVET, AKA "BROKEN PIN RIVET" WORK?
 

A blind (or “pop”) rivet is so-named because it can be fixed "blind", that is to say without having access to one of the two sides of the assembly. It consists of two parts: the body (a hollow tube with a head also called a flange) and the nail (a rod responsible for deforming the body during crimping). To rivet:


• use a riveting pliers
• pull the selected nail with the riveting pliers
• the swollen part of the nail will then enter the body until the nail breaks

• the rivet remains fixed in place (hence “broken rod rivet”).
 
 

DETERMINE THE RIVET TO USE: ALUMINIUM OR STAINLESS STEEL, LARGE OR COUNTERSUNK HEAD, ETC.
 

Are you looking to identify the most suitable blind rivets for your project? Remember that there are several parameters to consider, namely:


• the material of the nail (aluminium, steel, stainless steel, copper ...), which depends on the load to be supported and the material of the part to be crimped, to reduce the risk of corrosion
• the rivet head (classic flat head for hard materials, wide head reserved for softer materials, countersunk head for an impeccable finish ...)
• the diameter of the body of the rivet, which must correspond to the diameter of the hole minus 0.2 mm
• the thickness of the part to be crossed, knowing that the rivet must not be too short, but must not exceed
• and of course the type of rivet, as we will see in the next paragraph.
 


FLUTED, EXPLODED, PETAL BLIND RIVET… DISCOVER OUR DIFFERENT MODELS
 

At Würth, we have designed multiple models of blind rivets, adapted to all the needs encountered by professionals who frequently perform riveting. Visit our online store and you will find rivets with various bodies:


• blind structural rivets, used for parts subject to strong vibrations and high shear stresses, perfect for making hyper-resistant assemblies, for example for machines or truck bodies
• fluted blind rivets, with fluted bodies which facilitate their fixing in wood or plastic
• exploded blind rivets, which open in four parts, lose their heads during installation and are intended for fragile materials
• petal blind rivets, quite similar to exploded rivets, but which retain their heads during crimping and whose opening takes the form of three petals, etc.